What is the cable to connect a HMISTU to a Momentum PLC?

Article available in these languages: japonština

Issue:
Need to determine what cable is used to connect a HMISTU to a Momentum PLC?

Product Line:
Magelis (HMISTU/HMISTO/XBTGT/XBTGK/XBTGH/HMIGTO/HMIGTU)

Resolution:
The cable diagrams listed in the Modbus RTU driver manual of Vijeo Designer for this connection are:

XBTZG939 + XBTZ9711 for RS232 Communication
VW3A8306R10 For RS485 Communication.

NOTE: These cables do not apply for the 171CBU78090

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: