What does RDY status on an Altivar drive mean?
Issue:
RDY status on an Altivar drive.

Product Line:
All Altivar drives

Environment:
All models currently in production, all serial numbers.

Cause:
Customer is unsure what this code indicates

Resolution:
RDY is an indication that the drive is ready to run and has not detected any faults, but does not currently have a command to run.  This is the normal status of the drive when it is powered, but does not have a run command present, or any other logic inputs triggered to disable the drive, such as a freewheel stop input or external fault input.

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: