Questions on where to ship 3 phase batteries for disposal

Issue:
Questions on where to ship 3 phase batteries for disposal

Product line:
3 Phase cartridge batteries

Environment:
All 3 phase modular battery units.


Resolution:
For disposal of batteries used in 3 phase product applications Schneider only provides pre-paid shipping labels for batteries that are either under their initial 1 year warranty or for batteries being replaced as part of a specific battery contract.

Customers are welcome to ship batteries to the following address for proper disposal of 3 phase related batteries –
Schneider Electric
201 Fulling Mill Rd, Middletown, PA 17057

Note –
  • For all 3 phase batteries the customer is required to pay for the return ship of any battery that is not under warranty or specific Battery Service contracts.
  • Customers may arrange their own heavy weight pick up if desired thru major shipping companies.
  • Schneider does not provide packaging for returning batteries.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: