What is the difference between the Altivar 61/71 drives and the Altivar 61/71 Plus drives?

Issue:
Differences between the Altivar 61/71 drives and the Altivar 61/71 Plus drives.

Product Line:
ATV61/71 series

Environment:
All serial numbers for ATV61/71 series

Cause:
N/A

Resolution:
The Altvar 61/71 drives are open style IP20 rated drives meanwhile, the Plus drives are UL type 12 Enclosed drives that start at 125HP.
Please reference the attachment for additional information on the Altivar 61/71 Plus Drive series.

Schneider Electric Česká republika

Přílohy

30072-454-96.pdf30072-454-96.pdf [5.74 MB]
Zjistěte více
Řada:
Zjistěte více
Řada: