Can a port number other than Modbus/TCP port 502 be used for I/O Scanning on the 140CPU6xxxx native ethernet port?

Product Line:
Quantum PLC

Environment:
EcoStruxure Control Expert

Resolution:
No,
the Quantum 140CPU6xxxx Copro native ethernet port will only use Modbus TCP port 502 when performing an I/O Scanning function.
Port 502 is hard-coded into the Ethenet port settings and is not configurable.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: