Video: How to reset the Vijeo Designer layout back to default?

Issue:
Looking for a way to reset my Vijeo Designer windows. The Windows are all scattered.

Product Line:
Vijeo Designer (all versions)

Resolution:
Sometimes when you move the windows and panes around in Vijeo Designer, you may want to move them back to default. The easiest way to do so is with the following procedure:

Simply shutdown Vijeo Designer, open up REGEDIT and delete the following key:
-For Vijeo Designer v6.2 SP8 or older, delete:
HKEY_CURRENT_USER\Software\Schneider Electric\Vijeo-Designer62

-For Vijeo Designer v6.2 SP9 or newer, delete:
HKEY_CURRENT_USER\Software\Schneider Electric\Vijeo-Designer62B

After you delete that, restart Vijeo Designer.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: