Which Modicon TSX Quantum CPUs are supported in Concept? and Which are supported in Unity Pro?

Article available in these languages: Španělština

Issue
To proper support PLC based Automatic Transfer Scheme/MicroGrid Control/Load Sharing systems, it's beneficial to understand what programming software can be used to program the long lived Modicon TSX Quantum platform.

Product Line
Modicon TSX Quantum

Environment
Programming Modicon TSX Quantum

Cause
Programming tool for Modicon TSX Quantum shifted from Concept to Unity Pro.

Resolution
The following CPU Models are programmable by Concept:
1. 140CPU11302
2. 140CPU11303
3. 140CPU21304
4. 140CPU4240x
5. 140CPU43412
6. 140CPU43412A
7. 140CPU53414
8. 140CPU53414A

The following Modicon TSX Quantum CPU can be programmed by Unity Pro:
1. 140CPU31110
2. 140CPU43412A
3. 140CPU43412U
4. 140CPU53414A
5. 140CPU53414U
6. 140CPU65160
7. 140CPU65160
8. 140CPU65260
9. 140CPU67160
10. Safety CPUs

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: