What all Timer parameters are available in PM2200 series energy meter ?

The meter supports an active load timer, meter operation timer, and run hour.

Active load timer
Active load timer shows how much time a load has been running, based on the
specified minimum current for the load timer setpoint setting.

Meter operation timer
Meter operating timer shows how long the meter has been powered up.

Run Time
Run time shows how much time a load has been running, based on accumulated
energy - received and delivered.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: