Does PME for Health Care come with EPSS?

Issue:
A customer would like to know if the EPSS module is installed with PME for Health Care Edition.

Product Line:
Power Monitoring Expert for Health Care 8.x

Environment:
EPSS Module

Resolution:
The EPSS module is installed with PME for Health Care, but requires an activation ID for licensing before it can be used. The commissioning process differs for systems which do and do not use the EPSS module. For commissioning information refer to article FA284199.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: