What is the current consumption (burden) of IRIG-B port in ION 8650 meter?
Product Line
ION8650

Environment
Hardware

Resolution
The input impedance on the IRIG-B port (red to black) is 450 kΩ. So for a 5 V input voltage, the current draw would be around 0.01 mA.

Schneider Electric Česká republika