Follow these steps to upload Advantys island configuration(STB NIP <example>) through TCP/IP.
1. Open the Advantys software and provide a new workspace & file name.
2. Go to online > Click connection settings.
3. Select connection type as TCP/IP and enter the IP address of Advantys STB NIP <example> module.
4. Then Click connect > Upload button to start uploading the configuration.
Publikováno pro:Schneider Electric Česká republika