{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
What is the size of the cutting in partition wall for passing through a Canalis KS element?
For easy handling and installation a 50mm distance to the wall on each side of the KS element should be considered.

Two rules have to be followed for correct installation:
- No junction block at level of partition, for maintenance purpose;
- If at the level of partition the cutting in the wall will be filled with plaster, it must not be on a tap-off outlet.

Schneider Electric Česká republika

What is the size of the cutting in partition wall for passing through a Canalis KS element?
For easy handling and installation a 50mm distance to the wall on each side of the KS element should be considered.

Two rules have to be followed for correct installation:
- No junction block at level of partition, for maintenance purpose;
- If at the level of partition the cutting in the wall will be filled with plaster, it must not be on a tap-off outlet.