TeSys T LTMR..EBD doesn't respond to network commands
Issue:
Tesys T does not respond to command via Ethernet. IP address can be pinged, registers can be read, and Tesys is configured for network control but will not respond to network commands.

Product Line:
LTMR Tesys T motor controllers.

Environment:
Products sold in the US

Cause:
Tesys was in configuration mode, not run mode.

Resolution:
The Tesys will not run in configuration mode. In run mode you only have command menu under the device tab in the latest DTM Library. Ensure you have the latest DTM Library Installed. This will allow you to place Tesys in Run mode and verify proper operation.

Schneider Electric Česká republika

Zjistěte více
Produkt:
Řada:
Kategorie:
Užitečné články
Zjistěte více
Produkt:
Řada:
Kategorie: