Can troughs install across the rear of the new NetShelter roof?
Issue:
It appears that troughs can't install across the rear of the NetShelter roof.

Product Line:
NetShelter SX

Environment:
AR3100, AR3300, AR3150

Cause:
Some of the trough mounting holes are missing.

Resolution:

Troughs can also be installed by connecting them to the adjacent trough. Please see page 1 of the Installation Instructions.
Also, see the attached file.

Schneider Electric Česká republika

Přílohy
20180423 New NetShelter Roof Trough Installation in Rear Rev 2.pdf [423.79 KB]
Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: