Video: Making a switch in Vijeo Designer that remains down while the bit is high
In Vijeo Designer, we must make use of two objects to animate a switch that stays down while the bit is high and that is also able to reset the bit when touching it.

We make use of:
1) A radio button (to set the bit and to stay down when the bit is high)
2) An invisible switch to be used to reset the bit. The switch has a visibility condition to only appear when the bit is high.

Please see the following video for a demonstration of this procedure:

Schneider Electric Česká republika

Přílohy
DownStateSwitch.zip [17.51 KB]
Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: