{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Prohledejte časté dotazy
What are inputs JerkRatio1-2-3-4 of MC_MoveVelocity_PTO ?
In Ecostruxure Machine Expert, the function block MC_Movelocity_PTO has 4 JerkRatio inputs.
-

JerkRatio1-4 are used to change the shape of the S-curve.

-
 
  • JerkRatio1: Percentage of acceleration from standstill used to create the S-curve profile
  • JerkRatio2: Percentage of acceleration to constant velocity used to create the S-curve profile
  • JerkRatio3: Percentage of deceleration from constant velocity used to create the S-curve profile
  • JerkRatio4: Percentage of deceleration to standstill used to create the S-curve profile