How do we enable the mouse and keyboard control on an iPC for Vijeo Designer Runtime?
Issue:
How do we enable the mouse and keyboard control on an iPC for Vijeo Designer Runtime?

Product Range:
Vijeo Designer Runtime for Windows

Resolution:
In order to enable the mouse and keyboard control on an iPC with Vijeo Designer Runtime, you will need to make the setting change to the properties below:
Windows Control
- Disable Key Control --> Disabled
- Hide Mouse Cursor --> Disabled

If you do not have the source file for the Vijeo Designer application file, you can make a change to a configuration file (Project.cfg) found here:
C:\Program Files\Schneider Electric\Vijeo-Designer\Vijeo-Runtime\public\

Set the following entries:
DisableTaskBar=0
HideMouseCursor=0

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: