Are NetShelter Performance Cable Managers and Valueline cable managers compatible with the CPI Universal Rack?
Issue:
We have been asked to confirm compatibility between the CPI Universal 2-post rack and NetShelter Performance or Valueline vertical cable management.

Product Line:
NetShelter 2-Post Rack

Environment:
All versions and serial ranges.

Cause:
Some of the CPI 2-post racks have a higher load rating than the NetShelter.

Resolution:

The mounting holes on the NetShelter Performance and Valueline Cable Managers align with the mounting holes of the CPI Universal 2-post racks, so they are compatible.
NetShelter Performance and Valueline Cable Managers are compatible with the following CPI Universal 2-post racks:
46353-Series
48353-Series
46383-Series
48383-Series


The names Chatsworth and CPI are registered trademarks of Chatsworth Products Inc.

Schneider Electric Česká republika

Zjistěte více
Řada:
Užitečné články
Zjistěte více
Řada: