Issue
When trying to build an M340 project the error "{Device (x.x) BMX AMx 0<example>}: IODDT "<example>" not compatible with State RAM mode." is reported.
Product line
Unity Pro, Control Expert, Modicon M340
Resolution
This error occurs if the IO modules are mapped as State RAM and the project is trying to use the T_ANA_IN_BMX IODDT. This is not allowed. There are certain components that can be used, but not the IODDT in it's entirety.
Publikováno pro:Schneider Electric Česká republika