Before on M340 local drop , we have a solution as there are Modulo Value and Present Value.But we don’t find the counterpart value when BMXEHC0200 is configured at M580 RIO drop so that we could not retain the last value following power restart of BMXEHC0200.

BMXEHC0200 on M580 RIO drop. These two values are present in the IODDT while they are not available in the DDDT. So we could not use the application to write back the last value of BMXEHC0200 after repowering when it is configured at M580 RIO drop. The FAQ also applies when BMXEHC0200 is configured at the M580 local drop.
Publikováno pro:Schneider Electric Česká republika