how to display the Motor rotation direction on the Altivar ATV12 frequency inverter integrated HMI?

By default setting, when the drive is running, the default value displayed is the motor Output frequency rFr.
The monitoring parameter displayed on HMI can be changed to one of the monitoring parameters (Monitoring mode - STAT)
This STAT (product status) will display status (rdy, run, ACC, dec, ....). When motor is running there will be "run" on HMI + direction of rotation.
See attached page from manual that mentions last 6 segments will provide direction of rotation.
Direction of rotation is also present in ACC and DEC state.
Segments shows fwd direction when segments are moving cw (clock-wise), reverse direction when segments moves ccw (counter-clock wise)

Schneider Electric Česká republika

Přílohy

ATV12_direction_on HMI.jpgATV12_direction_on HMI.jpg [292.05 KB]
ATV12_direction.zipATV12_direction.zip [53.28 KB]
Zjistěte více
Řada:
Zjistěte více
Řada: