undefined undefined
{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Vijeo Designer 6.2 cannot launch after updating to Windows 10 build 1903
Issue:
After upgrading to Windows 10 Build 1903, Vijeo Designer V6.2 no longer launches and gives error code (0xc0150002).

Product Line:
Vijeo Designer (all versions)

Resolution:
Upon updating to Windows 10 Build 1903, Vijeo Designer 6.2 may fail to launch. The new update provided by Microsoft somehow disturbs the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries required by Vijeo Designer. The solution is to re-install the Microsoft Visual Studio 2005 SP1 C++ Redistributable libraries using the attached file installation package.

NOTE: Windows 10 build 1903 may also block running any file that did not originate from the Microsoft App Store. To workaround this, you will need to goto Settings->Apps->Apps & Features and change the setting for "Choose where to get apps" from "The Microsoft Store only (recommended)" to " Anywhere".
Apps menu
Please find the needed file attached to this FAQ document.
 

Schneider Electric Česká republika

Přílohy
vcredist_x86.exe [2.62 MB]