undefined undefined
{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Is it possible to control (start up or shut down remotely) either Galaxy VM and Galaxy VX UPS operation via NMC command/NMC?

Article available in these languages: Španělština

Product Line: Galaxy VM and VX

Environment: All Models

Answer: No, it is not possible to control the Galaxy VM and VX UPS operation via NMC remotely on the network.

Schneider Electric Česká republika

Is it possible to control (start up or shut down remotely) either Galaxy VM and Galaxy VX UPS operation via NMC command/NMC?

Article available in these languages: Španělština

Product Line: Galaxy VM and VX
 

Environment: All Models
 
Answer: No, it is not possible to control the Galaxy VM and VX UPS operation via NMC remotely on the network.