undefined [object Object]
{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Easergy P5 P5x30 and P5x20: Is there a flush mounting accessory for the relay?
Easergy P5 can be installed with or without a flush mounting accessory. Using the flush mounting accessory helps to reduce the installation time thanks to the automatic fixing system and to achieve IP51 from the the front.

The following references are available:
REL51032: 20TE
REL51052: 30TE

Schneider Electric Česká republika

Easergy P5 P5x30 and P5x20: Is there a flush mounting accessory for the relay?
Easergy P5 can be installed with or without a flush mounting accessory. Using the flush mounting accessory helps to reduce the installation time thanks to the automatic fixing system and to achieve IP51 from the the front.

The following references are available:
REL51032: 20TE
REL51052: 30TE