{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Prohledejte časté dotazy
When using preset speeds and an analog speed input which one takes priority?
When the inputs for the preset speeds are high they override the analog speed. If the preset speed inputs are low then the drive will run at the analog speed input speed or LSP if no signal is present.


CTA-ID : 2001374

Schneider Electric Česká republika

When using preset speeds and an analog speed input which one takes priority?
When the inputs for the preset speeds are high they override the analog speed. If the preset speed inputs are low then the drive will run at the analog speed input speed or LSP if no signal is present.


CTA-ID : 2001374