Issue:
Can I directly substitute an ATV930 from ATV71 on CANopen network?
Product Line:
ATV71, ATV930
Environment:
Altivar
Resolution:
There is no direct substitution from ATV71 to ATV930. But it’ i possible to configure the ATV930 CANopen PDO to have the same data as ATV71. In order to replace ATV71 by ATV930 on CANopen, you first need to define the ATV930 inside the catalog manager.
See link below for FAQ and ATV930 CANopen manual.
https://www.se.com/ww/en/faqs/FA320804/
Publikováno pro:Schneider Electric Česká republika