What temperature conditions can the ATV630 / ATV930 drives be stored in?

Issue:
What are the environmental temperature conditions for ATV630 / ATV930 drive storage?

Product Line:
ATV630
ATV930

Environment:
All frame sizes

Cause:
Customer stock

Resolution:
All drives other than frame sizes 7, and floor standing products

Ambient storage temperatures:
°C -40...70
°F -40...158

Frame sizes 7, and floor standing drives
°C -25...70
°F -13...158

All drives relative humidity   5…95%
All drives storage must be dry and free from dust.

Schneider Electric Česká republika

Zjistěte více
Řada:
Zjistěte více
Řada: