How is the communication time out managed when using an Ethernet option card with the ATV600 series drive?
Issue:
The RPI setting does not appear to impact the Communication timeout as described in the option card manual.

Product Line:
Altivar 600 series drives: ATV630, ATV650, ATV660, ATV680 when using Ethernet option cards VW3A3720 or VW3A3721

Cause:
Documentation needs updated

Resolution:
The communication timeout related to the Ethernet option card is an internal parameter TOUT (register 64211, units are 0.1 seconds).
This parameter can be accessed using SoMove by adjusting the Holdup Time under the Modbus TCP settings in the option card tab.  The time set applies to both Modbus TCP and Ethernet IP communications.

Attach Video here:

Schneider Electric Česká republika

Zjistěte více
Produkt:
Řada:
Užitečné články
Zjistěte více
Produkt:
Řada: