Can the OFS Server communicate to an M580 via the USB port?
Issue:
OFS server communication to M580 USB port


Product Line:
OFS Server, M580


Resolution:
Yes, OFS Server can communicate to an M580 PLC via the USB port. To configure the OFS server to communicate to the M580 via USB, launch the OFS configuration tool. Then create an alias by selecting "File"  then "New Device Alias". Next click on the ellipsis for Device address 1 to add the USB driver. Select M580 for the Device type and add the symbol table file. Save the configuration.
sdc

Select USB driver from the list and then select OK.
image2

Schneider Electric Česká republika

Zjistěte více
Produkt:
Užitečné články
Zjistěte více
Produkt: