How to find PLC and Memory load of BMED581020 PLC (IEC 61499) by application
You must used “MIBGET” function block.
mibget
Where is the list of “MIBGET” functionality?
mibget list
For CPU load:
CPU load
For Memory:
memory load

Example of application with CPU load:
  • Add “MIBGET” function block like this
application mibget
  • Change parameter VALUE1 “STRING” to “UDINT” of “MIBGET” function block
mibget parameter
mibget parameter
  • Save + Compile + deploy + RUN your application
  • Generate event on REQ => result of value is 118 => CPU load = 11.8%
mibget result

Product line:
EAE, CPU load, Memory load, MIBGET, Simulator, BMED581020, IEC 61499
Environment:
Windows, EcoStruxure Automation Expert 22.0

Schneider Electric Česká republika

Zjistěte více
Produkt:
Řada:
Užitečné články
Zjistěte více
Produkt:
Řada: