{}

Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
Jak vám dnes můžeme pomoci?
Control Power Transformers 3kVA and 5kVA should be installed on its own instrument compartment?
Issue: 
Control power transformers: 3 and 5 kVA on its own instrument compartment. 
Product Line:
Power Zone 4 Switchgear and QED6 Switchboard
Environment:
Power Products
Cause:
Can be installed additional components no associated to 3kVA or 5kVA transformers and primary and secondary protection in same instrument compartment?
Resolution:
Investigated with UL File - Vol SQ section General, Transformers rated 3000-5000VA shall be mounted in a compartment, otherwise empty, of minimum dimensions 21 by 21 by 15 in. so as long as we can meet that min. space for that application, a compartment may be shared with small components that don't protrude that space.