Power Monitoring Expert (PME) Web shows "Service Unavailable: HTTP Error 503. The service is unavailable."

Issue
The following error is shown when attempting to open PME web:  
Error appears in a web browser that reads: "Service Unavailable: HTTP Error 503. The service is unavailable."
"HTTP Error 503. The service is unavailable." The error appears whether or not the fully qualified domain name is used or localhost is used. Other PME applications (management console, vista, designer..) are functional.
 
Product Line 
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
 
Environment
PME Web Applications
IIS Manager (inetmgr)
 
Cause 1
The PME installer enables and configures the Internet Information Services (IIS) to host the different Web Applications. When the "Application modules App Pool" is disabled in the IIS, it causes a 503 error to appear when attempting to open Web applications.

Cause 2
An application or a process is using the port 80 (HTTP) or port 443 (HTTPS).
 
Resolution 1

  1. Open the IIS Manager
  2. In the "connections" pane, click on the arrow key next to the server name to extend the tree
  3. Click on "Application Pools"
  4. Highlight the "Application Modules AppPool"
  5. Right click and select "start," to start the App pool. Alternatively, press "start" in the "Actions" pane
  6. Return to PME web and refresh the page.

 
Resolution 2
Please refer to the resolution in FA405661.

Schneider Electric Deutschland

FAQ-Nutzungshinweis

Bitte lesen Sie sich die Bedingungen für die FAQ genau durch. Sie müssen den Bedingungen zustimmen, bevor Sie mit der Suche beginnen können.

Die in den FAQs aufgeführten Antworten dienen als Hilfestellung und Orientierung. Es besteht kein Anspruch auf Vollständigkeit und Aktualität. Sie ersetzen nicht die AGBs, die Technischen Dokumentationen, die Gebrauchsanweisungen, die Sicherheitshinweise und die anerkannten Regeln der Technik.

move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.