What size fuses are used in the ATS48 for the control circuit going to CL1 and CL2?
Issue:
ATS48 fuse size for circuit control going to CL1 and CL2

Product Line:
Altistart 48, ATS48

Environment:
All open style units.  All models, All Serial numbers.

Cause:
Selection of Fuses.

Resolution:

ATS48D17Y and ATS48D22Y we recommend Class CC 600V 0.5 A fuses.

ATS48D32Y, ATS48D38Y, ATS48D47Y, ATS48D62Y, ATS48D75Y, ATS48D88Y, ATS48C11Y, ATS48C14Y, and ATS48C17Y we recommend Class CC 600V 0.6 A fuses.

ATS48C21Y, ATS48C24Y, and ATS48C32Y we recommend Class CC 600V 1.0 A fuses.

ATS48C41Y, ATS48C48Y, ATS48C59Y, ATS48C66Y, ATS48C79Y, ATS48M10Y and ATS48M12Y we recommend Class CC 600V, 1.5 A fuses.

See attached file.  Information provided in Table 31 (page 83) of document S1A37491 Altistart 48 Y-range Soft Start Controllers Instruction Bulletin.

Schneider Electric Danmark

Bilag
ATS48 Control Fuse Ratings.pdf [93.72 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: