Where are the Control Coil Terminals for TeSys D Line Contactors?

Issue:
Control coil terminal marking and location on Tesys D Line  contactors

Product Line:
Contactors and Starters-IEC

Environment:
TeSys D Contactors

Resolution:
The coil terminals are marked A1 and A2, you can see them on the front of the contactor. They are next to the auxiliary contact (13/14 NO, 21/22 NC) terminals.
For DC Coils, positive and negative terminals are marked. A1 for positive, A2 for negative.

Schneider Electric Danmark

Se mere
Produkt:
Område:
Se mere
Produkt:
Område: