Are the 9001K51 and 9001K52 Closing Plates Metal or Plastic?
Issue:
Clarifying is the closing plates are metal or plastic

Product Line:
9001 30mm

Environment:
North American Products

Resolution:
Both 9001K51 and 9001K52 are plastic.  They do come with a metal ring nut that secures the closing plate to the back of the enclosure.
Meets UL and Nema 1, 2, 3, 4, 4x, 6, 12, and 13.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: