Søg i ofte stillede spørgsmål
Is the Automatic adaptation of deceleration ramp feature available in Altivar 61 drive.
Automatic adaptation of deceleration ramp feature is available in Altivar 61 drive.
It assists in prevention of over voltage fault, in case the user has set the deceleration ramp value very low for the high load inertia applications, by automatically adapting the deceleration ramp.
brA [Dec Ramp Adapt.] = Yes (It is a factory default setting).
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: