Does Schneider Electric offer Altivar VFD in a NEMA 4 enclosure?
Issue:
Are Altivar VFD available in NEMA 4 enclosures?

Product Line:

All

Environment:
NEMA 4 enclosure

Resolution:
Altivar drives standard offering includes Type 1, 12, and 3R enclosure ratings.  Custom units including Type 4 and 4X typically can be built to order.  Contact your local distributor or SquareD sales office to request a quotation from the Engineered Drive solutions team.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: