Is there a limitation on the length of load conductor that can be used with AFI ,CAFI, and Dual Function breakers?
Issue:
Length of cable run for AFI, CAFI, or DF circuit breakers.

Product Line:
Advanced Function Circuit Breakers

Cause:
Excess cable length may interfere with circuit breaker operation.

Resolution:
The maximum length of branch circuit wiring should be no more than 250ft.

Schneider Electric Danmark

Se mere
Område:
Se mere
Område: