Søg i ofte stillede spørgsmål
TVSS (SPD - Surge protective Device) in Model 6 MCC: Is the flange-mounted disconnect a 30A?
Yes, the 30A GJL36030 circuit breaker If the unit was manufactured prior to November 2012. After October 2012, the TVSS, now referred to as an SPD unit was manufactured with a Bladed Switch disconnect or no disconnect at all. GJL36030 is now obsolete, for units prior 2012 replacements contact your Local Schneider Electric Sales office.
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: