Dew Point Calculations on the NetBotz Appliances
Issue:
Dew-Point Calculations on the NetBotz Appliances

Product Line:
NetBotz

Environment:
NetBotz version 1 and 2

Cause:
Definition: Dew Point is the temperature at which condensations forms

Resolution:

When air comes in contact with a surface that is at or below its Dew Point temperature, condensation will form on that surface.

The following external site explains how the dew point is calculated: http://www.dpcalc.org/

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: