What is the operating temperature range of the ATS01 soft starters?
Issue:
What is ATS01 soft starter operating temperature?

Product Line:
ATS01

Environment:
All series

Causes:
N/A

Resolution:
The ATS01 soft starters are rated for use in ambient temperatures ranging from -10C (14F) to +40C (104F).  The starter can be used up to 50C (122F) by derating the current by 2% per degree C above 40C.

The obsolete ATS01N2**LY were rated for use in ambient temperatures ranging from 0C (32F) to +55C (131F).

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: