Why is notify users missing or grayed out in PowerChute Network Shutdown on my Windows system?

Issue:
Notify users is missing or grayed out in PowerChute Network Shutdown on my Windows system.

Product Line:
PowerChute Network Shutdown

Environment:
Windows Vista, 7, 8, 2008, 2010, 2011, 2012, 2016, 2019, Hyper-V, 2022, 2025, Azure HCI

Cause:
Starting with the release of Windows Vista, Microsoft removed the messaging service from their OS. PowerChute relied on this messaging service.

Solution:
1 - A third party messaging service can be scripted to send messages.

2 - Review Kbase Messaging service for PowerChute Network Shutdown running on Windows.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: