Can the default control board for the ATV212 (or ATV21) drive be purchased as an individual part?
Issue:
Control board for the ATV212 (or ATV21) drive replacement

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
Needs to replaced the basic control IO card that was in the ATV21 or ATV212 drive.

Resolution:
No. This part is not available to purchase in the US.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: