Can I replace an ATV21 drive in an SFLEX with a ATV212 drive?
Issue:
Replace an ATV21 S-Flex Drive.

Product Line:
Altivar 21 ATV21

Environment:
All models, All series

Cause:
Inoperative ATV21 drive in an SFLEX enclosure. Need to replace the ATV21 power converter.

Resolution:
Yes, you can replace the ATV21 drive with a ATV212 (same size)  drive inside the S-FLEX enclosure.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: