How do I change the contrast and stand-by time on the ATV61 and ATV71 keypads?

Issue:
Wanting to  change the contrast and stand-by time on the ATV61/71 keypads.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Adjust contrast or set up keypad stand-by mode to turn off HMI backlight.

Resolution:

  • Go to Main menu
  • Select menu 7 Display Config
  • Select menu 7.4 Keypad Parameters
  • Go to Contrast and Stand-by settings and make necessary adjustments.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: