Where can I find the RJ45 pin out for the ATV61/ATV71 drives?
Issue:
RJ45 pin out for ATV61/71 drives

Product Line:
All

Environment:
All

Cause:
Can not find documentation

Resolution:
The RJ45 connector uses two wire RS-485 connection for Modbus communications.
Pin 4 is the DB (+). Pin 5 is DA (-). These terminals are for communication.
Pin 7 is 10 VDC and 8 is 0 VDC. These are used to power the remote keypad when connected to this drive or the RS232 to RS485 adaptor when connecting from a PC with Powersuite.
The pins are numbered from Right to Left when looking at the front of the drive.

Schneider Electric Danmark

Bilag
Altivar 71 Intergrated Modbus 09080512142096779.pdf [657.85 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: