Are the NetShelter SX Cabinets grounded per UL / IEC 60950, 61010-1 / 6.5.1.3?
Issue:
Customers require information on grounding NetShelter cabinets to IEC specifications.

Product Line:
NetShelter SX

Environment:

All versions and serial ranges.

Cause:

This installation requires grounding per IEC specifications.

Resolution :

NetShelter SX cabinets are UL Listed and have all metal components grounded per UL/IEC 60950 requirements and meet the 0.1 ohm resistance.
Equipment to be installed in a NetShelter SX cabinet should be Listed equipment.
Installation of any unlisted or recognized components requires a safety review of the completed assembly.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: