What is the replacement part number of the PCI SA85 Modbus Plus card P/N 416NHM3003x?

Issue:
Replacement part number of the PCI SA85 Modbus Plus card


Product Line:
Modbus Plus, 416NHM30030A, PCI SA85


Resolution:
The new part numbers for the PCI SA85 Modbus Plus network interface cards are:
Single Cable: Old number is 416NHM30030 and replacement is 416NHM30030A.
Dual Cable: Old number is 416NHM30032 and replacement is 416NHM30032A.

This card is an enhanced version of the older version of the card.
The new features are:

1.
The card will support the 3.3 and 5 volt PCI bus.
2.
The card will now mechanically fit in the PCI-X server bus slots. However it is up to the motherboard manufacturer if it will support the 33 Mhz operation of this card. The PCI-X bus runs at the speed of the slowest device installed, these cards run at 33 Mhz.
3.
The card will fit in both the PCI and PCI-X bus slots.
4.
The MBX Driver Suite will recognize the card as the 416NHM3003x. The card is backwards compatible with the MBX version 4.2b driver suite.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: