Søg i ofte stillede spørgsmål
What is the M340 clock accuracy?
Issue
Real Time Clock Accuracy
Product Line
Modicon M340
Resolution
The accuracy of M340 clock is:
At 25 °C : +/- 50 ppm or +/- 4.3 s by day.
From 0 to 60 °C : +/- 100 ppm or +/- 8.6 s by day.
Udgivet til:Schneider Electric Danmark
Se mere
Område:
Se mere
Område: