Søg i ofte stillede spørgsmål
What cable is used to connect a Harmony/Magelis HMI via RJ45 cable to Zelio Smart Relay Modbus module SR3MBU01BD?
Issue
What cable is used to connect a Harmony/Magelis HMI via RJ45 cable to Zelio Smart Relay Modbus module SR3MBU01BD?
Product Line
Zelio SR3 Smart Relays
HMI families with RJ45 ports: HMISTU, HMISCU, HMIGTO, HMIGTU, HMIST6, HMISTO715
Environment
Modbus Communication hardware
Resolution
Part number to connect Zelio Logic SR3 RJ45 (RS485 Modbus) to the RJ45 port of the HMIs from these families: HMISTU, HMISCU, HMIGTO, HMIGTU, HMIST6, HMISTO715 is either:
XBTZ9980 (2,5 m), or
XBTZ9982 (10 m).
These two cables have the same pinouts, but have different lengths.
Udgivet til:Schneider Electric Danmark
Se mere
Produkt:
Se mere
Produkt: